Produkt in den Warenkorb gelegt

What is the color temperature of a quartz halogen lamp and a metal halide lamp?

The typical color temperature of a typical quartz halogen lamp and bulb such as our 150W EKE Replacement Bulb is 3250 Kelvin, while that of a typical metal halide lamp and bulb such as our 100W Metal Halide Replacement Bulb is 5300 Kelvin. Spectral curves are available by visiting the presentation for each replacement bulb.

War dieser Inhalt nützlich für Sie?
 
Vertrieb & Beratung
1-800-363-1992
weitere regionale Telefonnummern
Einfaches
ANGEBOTSTOOL
Geben Sie zum Starten die Produktnummer ein.