Produkt in den Warenkorb gelegt

Danfoss: Edmund Optics Case Studies

Monitoring and regulating air pollution is an essential step towards creating a cleaner environment. Danfoss IXA, a high-tech company based in Denmark, is developing a device called MES 1001, a marine emission sensor based on ultraviolet absorption spectroscopy which monitors the NO, NO2, SO2 and NH3 emissions produced by cargo ships to ensure that they are complying with all environmental regulations. The optical sensor is placed inside the exhaust system of ships, so the involved optics will be exposed to extreme conditions and must be able to withstand temperatures up to 500°C and very high pressures simultaneously. Danfoss IXA was looking for a partner to develop optics fulfilling their demanding requirements, and in Edmund Optics® (EO) they found a partner who was prepared to take on this challenge which went beyond their normal capabilities. EO created custom test beds for verifying the unique requirements of the sensor, which enabled EO to develop a robust system to meet Danfoss IXA’s specifications. Danfoss IXA develops sensors and systems for the maritime industry, focusing on energy optimization and the measurement of emission gases. They are a part of the Danfoss Group, a global enterprise which produces a wide range of technologies that address a variety of markets including food supply, energy efficiency, and climate-friendly solutions.

War dieser Inhalt nützlich für Sie?

Produktübersichten

}
 
Vertrieb & Beratung
 
weitere regionale Telefonnummern
Einfaches
ANGEBOTSTOOL
Geben Sie zum Starten die Produktnummer ein.