Produkt in den Warenkorb gelegt

What are the advantages of Polarization Directed Lenses?

Polarization Directed Lenses are a thin film equivalent of a geometric optic. Thus, they have significantly less volume than an equivalent spherical optic, yielding significant reduction in weight and thickness. The technology used to create them is also well suited to create gratings and other polarization optics, allowing for multiple optical technologies to be designed into a single optical component.

War dieser Inhalt nützlich für Sie?
 
Vertrieb & Beratung
 
weitere regionale Telefonnummern
Einfaches
ANGEBOTSTOOL
Geben Sie zum Starten die Produktnummer ein.